Post Go back to editing

LT3439 Design

Category: Hardware
Product Number: LT3439

Hi,

I would like to use the LT3439 to create an isolated DC-DC converter with 5V input and bipolar output.

I need a very low ripple voltage so my idea is to connect at the output of LT3439 an LT3042 and LT3093.

I need a voltage +2.5V - 300mA / -2.5V - 300mA 

Please can you susggest to me suitable diodes and the transforme for my application?

My device is power safety so I would like to realize a voltage at the output of LT3439 enough for the dropout. 

Thanks in advance for your help.

Regards,
Carmelo

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.