Post Go back to editing

Issue with MAX17222ENT

Category: Hardware
Product Number: MAX17222ENT

Hello,

I am bringing up a new PCB design that uses the MX17222ENT device. The issue I am seeing is the device does not appear to be regulating the input voltage correctly. THe device is set up with a 191K RSEL resistor to achieve 3.3V output. When the input voltage is between 2 and 3 Volts the device produces 2.8V, when the input is raised to 4 Volts the output goes up to 3.6V.

Please advise what the issue may be.

Sid

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.