Post Go back to editing

efficiency of LTC3631 is too low

Category: Hardware
Product Number: LTC3631

I used LTC3631 on FPGA core power supply.When Vin is 6.4V,and Vout 1.2V/30mA,the efficiency of LTC3631 is only 73%.I want to know the max efficiency of LTC3631 in theory.I used LTSPICE,The tool can't detect LTC3631 steady state.Would you like to help me to simulate my schematic(LTC3631.asc).

The circuit of my physical board board is below,What  Parameter settings of peripheral  circuit can achieve the maximum efficiencyefficiency? 

 LTC3631.asc

Thank you very much.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.