Post Go back to editing

LTM4622 &LTM4705 Frequency Set for Dual Output voltage

Category: Hardware
Product Number: LTM4622 LTM4705

Hi 

We are using LTM4622 Dual Output Voltage part for Vout1 3.3V and Vout2 - 1.8V.

The datasheet specifies Frequency pin  : For 1.8V, FREQ Pin should be left open to set 1MHz and For 3.3V FREQ Pin to be connected ground with 324K to set 2MHz

Q1: In Two different output (LTM4622) Switching frequency Fsw of regulator will be same for both output, Right?

Q2: In my case, Where I've Vout1-3.3V and Vout2- 1.8V, What should be the Switching frequency set to?

If I set Fsw- 1 MHz, For 3.3V, Inductor ripple current as per the datasheet calculation, it results 2.392 A which is exceeding "1.2A peak-to-peak inductor ripple current" 

Same for LTM4705, Vout1-3.3V and Vout2- 1.35,

What should be Fsw?

Parents
  • Hello,

    What is your input/output requirement?

    Q1: In Two different output (LTM4622) Switching frequency Fsw of regulator will be same for both output, Right?

    Yes.

    Q2: In my case, Where I've Vout1-3.3V and Vout2- 1.8V, What should be the Switching frequency set to?

    If you insist on using the part numbers you mentioned, you should set the switching frequency to 2MHz to not violate the maximum peak current requirement.

    Regards,

    Jhun

Reply
  • Hello,

    What is your input/output requirement?

    Q1: In Two different output (LTM4622) Switching frequency Fsw of regulator will be same for both output, Right?

    Yes.

    Q2: In my case, Where I've Vout1-3.3V and Vout2- 1.8V, What should be the Switching frequency set to?

    If you insist on using the part numbers you mentioned, you should set the switching frequency to 2MHz to not violate the maximum peak current requirement.

    Regards,

    Jhun

Children