LT1170
Production
The LT1170/LT1171/LT1172 are monolithic high power-switching regulators. They can be operated in all standard switching configurations including buck,...
Datasheet
LT1170 on Analog.com
Hii Experts,
I have purchase LT1170 IC and i have Design PCB Board using datasheet Circuit Diagram.
I am giving Vin=32V and i am set Vout=12V but i am getting Vout= 29V i the circuit i am attaching my schematic diagram.
I have design circuit same in datasheet.
Please help me in this issue


Hi manoj1996,
in the attached circuit diagram, R6 and R7 are designed for an output voltage of approx. 5V. The reference design is not intended for an output current lower than 100mA. If in your measurement only R9 and LED3 draw some current, the output current is certainly below 100mA. Try increasing the output current above 100mA and measure the output voltage again.

Regards Michael
Ok Thank You I will change this
we need to keep r component how much value
has you said R9=20ohms i will keep led is in blue color
Thank you Output is Working
one more question
I am connecting 48V BMS Battery for PCB INput Voltage. We can give right