Post Go back to editing

ADP-I2C-USB for ADP1046A

Product Number: ADP1046A

Hello Support,

i have two questions regarding the programing of ADP1046A with the ADP-I2C-USB adapter.

1.: Where can I get the needed drivers for the ADP1046A? Windows shows me that i don`t have drivers for the ADP-I2C-USB adapter even after installing the GUI for ADP1046A.

2.: The datasheet of ADP1046A says a max. voltage of VDD+0.3V on the SCL and SDA pins and VDD is typical 3.3V. But the voltage of pin 1 of ADP-I2C-USB adapter is 5V.

Will there be any problems or can i safely connect the adapter like it is descirbed in the application notes?

Many thanks and kind regards.