Post Go back to editing

DATASHEET CLARIFICATION

Category: Datasheet/Specs
Product Number: LTM8067

Dear Ma'am/Sir

I would like use LTM8067 to derive 24V, where input voltage varies from 18V to 38V. Can i use LTM8067 in this scenaario? (Where as table:1 in LTM8067 datasheet shows that for 24V O/P max allowed i/p voltage is 21V).

otherwise please sujjest me any other part that can be used in the above specified conditions.

Thanks in advance.

Raja Manikanta

Parents
  • FormerMember
    FormerMember
on Mar 5, 2023 7:12 PM
0

Hello,

I would advise against using the LTM8067 as it has an absolute maximum of 25V and a 1V headroom might be too small.

I suggest using the micromodule below:

LTM8056 Datasheet and Product Info | Analog Devices

Regards,

Jhun

Reply
  • FormerMember
    FormerMember
on Mar 5, 2023 7:12 PM
0

Hello,

I would advise against using the LTM8067 as it has an absolute maximum of 25V and a 1V headroom might be too small.

I suggest using the micromodule below:

LTM8056 Datasheet and Product Info | Analog Devices

Regards,

Jhun

Children
No Data