Post Go back to editing

LTM8027 as Variable output voltage

Category: Hardware
Product Number: LTM8027

Hi,

 Can I use LTM8027 as variable output voltage source ?

I have 24V DC input and I want adjustable 2.5V to 12V with 3A output voltage controlled by DAC.

I don't want to add additional digital potentiometer on my board.

I have DAC which can give 4V FS.

As per datasheet range of RAdj should be from 56Kohm to 483Kohm.

RAdj=  56Kohm ( Vout 12V) and   RAdj=  483 Kohm ( Vout 2.5V)

Can you please tell me how to use this LTM8027 as a Variable output supply using DAC ? Is there any way to change output with the help of DAC ?

If any other Power supply module you want to suggest please suggest.

we need a solution (24V DC input and 2.5V to 12V DC output voltage with 3A output current) which requires less development efforts with minimal risks and part would be available easily in large numbers to procure for next 5-10 years.

Regards,

Bitesh