Dear ADI Expert,
In the Datasheet of MAX77827, there is only the description of the maximum output current as shown in the figure below: "With the 1.8A switching current-limit option, the IC can support up to 1.0A load current in buck mode and 900mA in boost mode (VIN = 3.0V, VOUT = 3.3V)". If 3.1A current-limit option is used, what is the maximum output current? Use the same 3.1A current-limit option, Vin=3V~5V, what is the maximum output current at Vout=5V?
Thanks & best regards.
Andy Yang.
added tag LMXMprodsupport
[edited by: GenevaCooper at 9:11 PM (GMT -5) on 21 Feb 2023]