Hi,
DC2374B Evaluation board has an Input Supply Range of 5V to 35V. Why? The LTC4013 has an Input Voltage Range of 4.5V to 60V
What do I have to do to have the input range specified in the LTC4013 datasheet?
DC2374B Charging options are ready for a 12V Battery. Can I use a 24V Lead Acid Battery with this demo board?
How? The LTC4013 datasheet claims that the Battery Voltage Range is 2.4V to 60V
Thanks in advance,
gaston