Post Go back to editing

Have a problem with the output voltage of the charge pump circuit, LTC3261. The output is lower than expected

Category: Hardware
Product Number: LTC3261

The circuittis as the one in the data sheet with the following components

CGA5L2X8R1E105K

Cap Ceramic 1uF 25V X8R 10% Pad SMD 1206 +150°C Automotive T/R

LTC3261MPMSE#PBF

High Voltage, Low Quiescent Current Inverting Charge Pump, 4.5 to 32 V Vin, 12-pin SOP (MSE-12-EDP), -50 to 150 degC, Pb-Free

C3225X8R1E106K250AC

Multilayer Ceramic Capacitors 10uF ±10% 25V X8R SMD 1210

The output voltages are as follows:

 

LTC

Temp

VIN

IIN

VO

TPlane

18oC

12V

40mA

-11.06

19.6

70

12V

40mA

-10.9

69.8

80

12V

40mA

-10.88

80.4

90

12V

40mA

-10.84

90.5

100

12V

40mA

-10.83

100.9

110

12V

40mA

-10.8

111

120

12V

40mA

-10.76

120.8

130

12V

40mA

-10.72

130.7

140

12V

40mA

-10.68

140.6

150

12V

40mA

-10.63

150.4

Can you please tell me why the output voltage is not the inverse of the input voltage.

  • Hello,

    The open loop resistance of the LTC3261 does get higher with temperature. The output voltage is about -(VIN - IOUT*ROL) where ROL is the open loop resistance. Below is the open loop resistance over temperature.

    With the temperature near 150°C the open loop resistance is close to 50Ω. This will create a voltage loss of about 2V. I would expect the output voltage to be about -10V with a 12V input and 40mA. At 18°C the open loop resistance should be over 30Ω. I would expect the voltage loss to be greater than 1.2V and the output voltage would be less than -11V in amplitude. These numbers are slightly better than what I would expect. 

  • Thank you. That answers my question.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.