LT8357
Recommended for New Designs
The LT8357 is a wide input range, current mode, DC/DC controller which can be configured as a boost, SEPIC or flyback converter. The LT8357 drives a low...
Datasheet
LT8357 on Analog.com
Hi,
I have designed a SEPIC converter, based on LT8357. I used the LT Power CAD and verified the design with excel sheet based on the datasheet.
The design spec is 9V-36V input, 15V output, 3A.
The problem is: When input voltage in <10.8V, output voltage drops to 5V.
My load is ~2A at 15V.

Any idea?
Ohad.