Post Go back to editing

LT8357 Sepic - not working at low voltage input

Thread Summary

The user designed a SEPIC converter using the LT8357 with a 9V-36V input and 15V, 3A output. The issue is that the output voltage drops to 5V when the input voltage is below 10.8V. The final solution involves using a 60V FET and a 4.7mOhm sense resistor, as the 40V FET and 8mOhm resistor limit the output power at lower input voltages. Additional troubleshooting steps included adjusting the EN/UVLO resistors and removing capacitors in parallel with the feedback dividers.
AI Generated Content
Category: Hardware
Product Number: LT8357

Hi,

I have designed a SEPIC converter, based on LT8357. I used the LT Power CAD and verified the design with excel sheet based on the datasheet.

The design spec is 9V-36V input, 15V output, 3A. 

The problem is: When input voltage in <10.8V, output voltage drops to 5V. 

My load is ~2A at 15V.

Any idea?

Ohad.

Parents
  • Hello,

    1. You have used a 40V FET -> in a SEPIC the Switch does see the sum of VIN and VOUT, hence 51V at 36V Vin -> You need a 60V FET. And the diode has to be a 60V type as well.

    2 With my approach LTpowerCAD suggests a Sense resistor of 4.7mOhm. You have chosen 8mOhm, hence you limit the possible output power at lower VIN.

Reply
  • Hello,

    1. You have used a 40V FET -> in a SEPIC the Switch does see the sum of VIN and VOUT, hence 51V at 36V Vin -> You need a 60V FET. And the diode has to be a 60V type as well.

    2 With my approach LTpowerCAD suggests a Sense resistor of 4.7mOhm. You have chosen 8mOhm, hence you limit the possible output power at lower VIN.

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.