KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LT8357
Recommended for New Designs
The LT8357 is a wide input range, current mode, DC/DC controller which can be configured as a boost, SEPIC or flyback converter. The LT8357 drives a low...
Datasheet
LT8357 on Analog.com
Hi,
I have designed a SEPIC converter, based on LT8357. I used the LT Power CAD and verified the design with excel sheet based on the datasheet.
The design spec is 9V-36V input, 15V output, 3A.
The problem is: When input voltage in <10.8V, output voltage drops to 5V.
My load is ~2A at 15V.

Any idea?
Ohad.
Hello Ohad,
Computing for your EN/UVLO divider resistor gives around 1.15V drop at 9V input. The drop should be >1.2V to turn on the device. Maybe try adjusting the UVLO resistors more and take in to account the hysteresis and tolerances.
Regards,
Jhun
Thanks for reply.
Even with EN/UVLO at 6V or EN tied to Vin, it still the same. The converter cannot supply the needed power
Some more info:
At Vin > 10.8V, switching signal to gate is ~2MHz . At low load (~100mA) it has low duty cycle, and while increasing load to ~2A, duty cycle gets higher.
At Vin < 10.8V, when load is low, ~100mA, switching signal to gate is 2MHz, with low duty cycle, and while increasing load to ~2A switching frequency decrease to 750KHz and voltage output drops down.
If I cycle the load, after several cycles it switches to 2MHz and works fine.
Ohad
Hello,
Can you try removing the capacitors you have in parallel with your feedback dividers and see if this improves? Also you have a high DCR on your inductor, have you tried simulating your design? If not, please do so. Thank you.
Regards,
Jhun
Hello,
1. You have used a 40V FET -> in a SEPIC the Switch does see the sum of VIN and VOUT, hence 51V at 36V Vin -> You need a 60V FET. And the diode has to be a 60V type as well.
2 With my approach LTpowerCAD suggests a Sense resistor of 4.7mOhm. You have chosen 8mOhm, hence you limit the possible output power at lower VIN.