Post Go back to editing

ADN8831 Vout2 vs Vtempset

Category: Hardware
Product Number: ADN8831

Hi,

I have aquirred the evaluation board and started to make some measurements. 

But first I have some doubts how to understand the datasheet and in that regard how the ADN8831 regulates.

Looking at this equation

V_out2 is equal to V_tempset when the wanted temperature is reached. I am not sure what exactly V_out2 is controlling, but later in the datasheet is another graph shown

So if my V_tempset is 1.25V then the voltage over the TEC is 0. But if I set my V_tempset to 0.5V then V_out2 is also 0.5V when the temperature is reached, but now the voltage over the TEC is not zero and it will still be heating or cooling.

Can someone explain if I have misunderstood something or if I have to always make my wanted temperature to a V_tempset=1.25V?

Thank you



minor typos
[edited by: tyassin at 7:39 PM (GMT -5) on 18 Jan 2023]
Parents Reply Children
No Data