ORING connected to DC-DC on the source and a battery bank on the drain. when the controller senses a positive voltage difference between the IN and OUT pins the controller turns on the MOSFETs.
Lets say I now want to turn off the controller. by the datasheet it will turn off when it senses a negative voltage of 25mV which is not good at all because it will never turn off on its own unless high reverse current will flow back into the ORING.
The datasheet suggest to disconnect the ground pin to turn off the controller but in this situation the output voltage is held high by the battery bank while the input voltage can drop down to 0.
The following picture dipicts the situation - Vout is big capacitor bank held at 58.5V.
ORING_IN is the DCDC output and can be shut down to 0V.
ORING_ON is now off and so the GND pin is floating.
will this safely turn off the ORING and the controller will remain undamaged?