Post Go back to editing

Replacement parts

Category: Hardware
Product Number: LTC3851
Software Version: -

I have a board which stopped working. There is an LTC3851 mounted (several ones). One of these is configured for a 3.3V Output. But at the Feedback pin I measure only approx. 0.2V instead of 0.8V. The Switch pin stays at around 1V and the pin with the internal Voltage at 5V is at 0.5V. So I think the part is broken. Now I’m looking for a replacement part. But I don’t know the exact type. It’s a SSOP so it should be LTC3851EGN or LTC3851IGN. There is also a mark 022 and another one with e3 on the Chip. The Datasheet says also: "The temperature grade is identified by a label on the shipping container", But I have none of these. Could you please tell me if it’s the Industrial or the extended temperature Range, or if not possible if I can simply take the Extended to be sure?

  • Hello,

    The temperature grade can not be determined from the part markings. Since you do not have the shipping container, then another option is to check the BOM or schematic for the full part number. If that information is not available and you do not know the actual temperature range, then use the LTC3851IGN (industrial grade) to be on the safe side. This version has a temperature range of -40C to +125C.

    Best regards,

    Mike

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.