Post Go back to editing

LT3591 - If - 300mA - is it possible to drive power led (If 300mA) with this chip?

Category: Hardware
Product Number: LT3591

Hi,

thinking, if the simple LT3591, with Uin from 3V-4,2V (single LiIon battery) can drive single power led, with If = 300mA?

The Rsense should be 0,6 Ohm. Ot it is limited to 100mA?

And what happened when the Uin will fall down below 3V?

best regards

M.M.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.