Hi,
Please tell me, LT8361 output minimun current.
Switching frequency minimum is 300kHz.
Is it possible 2mA/±80V output at 300kHz switching frequency?
Regards, Masa
LT8361
Recommended for New Designs
The LT8361 is a current mode DC/DC converter with a 100V, 2A switch operating from a 2.8V to 60V input. With a unique single feedback pin architecture...
Datasheet
LT8361 on Analog.com
Hi,
Please tell me, LT8361 output minimun current.
Switching frequency minimum is 300kHz.
Is it possible 2mA/±80V output at 300kHz switching frequency?
Regards, Masa
Looking from the efficiency figures of the typical applications from the datasheet, it can operate even under no load condition. Your specifications should be fine. There is also an available LTSpice model so you could try simulating it first.
Regards,
Nino
Looking from the efficiency figures of the typical applications from the datasheet, it can operate even under no load condition. Your specifications should be fine. There is also an available LTSpice model so you could try simulating it first.
Regards,
Nino
Hi, Nino
Thank you for your answering!
I'll it try.
Regard, Masa