Should the marking be 1764AEFE33 or LT1764AEFE-3.3?
In the datasheet the FE part marking is LT1764AEFE-3.3 but on the part that I have bought the part marking is just 1764AEFE33
Pay attention not just to the LT, there is not a dot between 3 and 3


LT1764
Production
The LT1764 is a low dropout regulator optimized for fast transient response. The device is capable of supplying 3A of output current with a dropout voltage...
Datasheet
LT1764 on Analog.com
Should the marking be 1764AEFE33 or LT1764AEFE-3.3?
In the datasheet the FE part marking is LT1764AEFE-3.3 but on the part that I have bought the part marking is just 1764AEFE33
Pay attention not just to the LT, there is not a dot between 3 and 3


Unfortunately, we are unable to provide information about parts in the EngineerZone community based on their markings. We suggest going back to your point of purchase to get this information. ADI only provides warranty coverage or any quality, reliability, failure analysis, applications, or other support on products purchased through ADI authorized distributors and sales offices. To ensure you are receiving unused, legitimate ADI products, please ensure all purchases are made through the ADI authorized distributors and sales offices listed on our website at Sales and Distribution | Analog Devices.
You can get more information on this topic on our website at Quality and Reliability Programs | Analog Devices.
Hi Emassa
There is a similar problem in HMC787 and a user ask his question about marking and there is an answer there.
Please pay attention to this link
Thank you for calling this thread to our attention. It will be removed as we do not answer part marking questions in the community. Please refer to the (+) Analog Devices EngineerZone Code of Conduct for more information.