Hi There,
I would like to know how I can wake up MAX17330 via either register/command or communication? FYI, I am able to wake it up using ALRT pin or by applying voltage source.
Thanks!
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
MAX17330
Not Recommended for New Designs
The MAX17330 is not recommended for new designs. The replacement part is the MAX17332.
The MAX17330 is a 28μA IQ stand-alone charger, fuel gauge, protector...
Datasheet
MAX17330 on Analog.com
Hi There,
I would like to know how I can wake up MAX17330 via either register/command or communication? FYI, I am able to wake it up using ALRT pin or by applying voltage source.
Thanks!
In order to wake the MAX17330 via register command/communication, you will need to first set the device to shutdown via the COMMSH bit in the Config2 (0ABh) register. This will shutdown the device and allow it to wake up upon the rising edge of any communication. See description of the bit below, which can be found on page 122 of the datasheet.
"COMMSH: Communication Shutdown. Set to logic 1 to force the device to enter shutdown mode if both SDA and SCL are held low. This also configures the device to wake up on a rising edge of any communication. See Table 9."
If the cell voltage is below 2.16V for any reason, than the part cannot be woken up by communication and must be awoken via a voltage source.