Dear All,
I am using LTC4263IDE as PSE controller in one of my project (Prototype) where as 48VDC required as POE .
I have verified my Schematic diagram w.r.t. Data sheet and Evaluation board design document.
I am getting always +48VDC at Out (Pin 9 & 10 ) w.r.t. Vss (Pin 5 & 6) even if i connect/disconnect POE PD (IEEE802.3af) , where I suppposed to get 48VDC_ Return.
(Note: My POE PD is working fine with other POE PSE circuit.)
My SD pin (Shut down) is high always.
I am using DC disconnect configuration in my design.
Kindly do the needful.
Thanks in advnce.
Regards,
Prabakaran P
Updated post with category
[edited by: GenevaCooper at 2:41 PM (GMT -5) on 19 Dec 2022]