Post Go back to editing

Question about LT8390

Thread Summary

The user inquired about using a single LT8390 for a 600W buck/boost output with 18V to 28V input and 24V, 25A output. The support engineer confirmed it is possible but would require bulky components and multiple MOSFETs, with a high inductor current (>30A saturation). LTpowerCAD was suggested for design assistance, and the user noted that simulations with recommended circuits only worked up to 300W output.
AI Generated Content
Category: Datasheet/Specs
Product Number: LT8390

Hi,

I am considering to use LT8390 with the following specs.

Vin=18V to 28V

Vout=24V, Iout=25A max  (Pout=600W max)

Is it possible to use a single LT8390 for 600W buck/boost output?  

If so, what precautions should be taken in circuit design?

If not, are there any products that can meet the above specs?

Regards,

Kazu

Parents
  • FormerMember
    FormerMember
on Dec 14, 2022 2:45 AM
0

Hello Kazu,

You can use LTpowerCAD to help you with your design requirement.

These are some of the controllers that were suggested by LTpowerCAD when inputting your specs.

Regards,

Jhun

  • Hi Jhun,

    I get the same products as yours for sure in LTpowerCAD except for LTC4020.

    I exported some recommended circuits showed in Power Stage Design to LTspice and simulated them, but they did not output 600W (24V/25A),

    They could work when the output current reduced to about 300W.

    Is it still difficult to achieve 600W output?

    Regards,

    Kazu

  • FormerMember
    FormerMember on Dec 14, 2022 7:00 PM in reply to Kazu
    +1

    Hi Kazu,

    600W is achievable but you would have bulky components. Plus, you would need >2 MOSFETs in your control and sync MOSFETs since it is a single phase.

    The datasheet has computation guidelines on how to compute for your desired specifications. I would think you'd need a high inductor current >30A saturation. I have ever only seen Wurth inductors having these.

    Regards,

    Jhun 

  • Reply
    • FormerMember
      FormerMember
    on Dec 14, 2022 7:00 PM in reply to Kazu
    +1

    Hi Kazu,

    600W is achievable but you would have bulky components. Plus, you would need >2 MOSFETs in your control and sync MOSFETs since it is a single phase.

    The datasheet has computation guidelines on how to compute for your desired specifications. I would think you'd need a high inductor current >30A saturation. I have ever only seen Wurth inductors having these.

    Regards,

    Jhun 

    Children
    No Data