Post Go back to editing

Question about LT8390

Category: Datasheet/Specs
Product Number: LT8390

Hi,

I am considering to use LT8390 with the following specs.

Vin=18V to 28V

Vout=24V, Iout=25A max  (Pout=600W max)

Is it possible to use a single LT8390 for 600W buck/boost output?  

If so, what precautions should be taken in circuit design?

If not, are there any products that can meet the above specs?

Regards,

Kazu

Parents
  • FormerMember
    0 FormerMember
on Dec 14, 2022 2:45 AM

Hello Kazu,

You can use LTpowerCAD to help you with your design requirement.

These are some of the controllers that were suggested by LTpowerCAD when inputting your specs.

Regards,

Jhun

  • Hi Jhun,

    I get the same products as yours for sure in LTpowerCAD except for LTC4020.

    I exported some recommended circuits showed in Power Stage Design to LTspice and simulated them, but they did not output 600W (24V/25A),

    They could work when the output current reduced to about 300W.

    Is it still difficult to achieve 600W output?

    Regards,

    Kazu

  • Reply
    • Hi Jhun,

      I get the same products as yours for sure in LTpowerCAD except for LTC4020.

      I exported some recommended circuits showed in Power Stage Design to LTspice and simulated them, but they did not output 600W (24V/25A),

      They could work when the output current reduced to about 300W.

      Is it still difficult to achieve 600W output?

      Regards,

      Kazu

    Children
    • FormerMember
      +1 FormerMember
    on Dec 14, 2022 7:00 PM in reply to Kazu

    Hi Kazu,

    600W is achievable but you would have bulky components. Plus, you would need >2 MOSFETs in your control and sync MOSFETs since it is a single phase.

    The datasheet has computation guidelines on how to compute for your desired specifications. I would think you'd need a high inductor current >30A saturation. I have ever only seen Wurth inductors having these.

    Regards,

    Jhun