Post Go back to editing

Question about LT8390

Thread Summary

The user inquired about using a single LT8390 for a 600W buck/boost output with 18V to 28V input and 24V, 25A output. The support engineer confirmed it is possible but would require bulky components and multiple MOSFETs, with a high inductor current (>30A saturation). LTpowerCAD was suggested for design assistance, and the user noted that simulations with recommended circuits only worked up to 300W output.
AI Generated Content
Category: Datasheet/Specs
Product Number: LT8390

Hi,

I am considering to use LT8390 with the following specs.

Vin=18V to 28V

Vout=24V, Iout=25A max  (Pout=600W max)

Is it possible to use a single LT8390 for 600W buck/boost output?  

If so, what precautions should be taken in circuit design?

If not, are there any products that can meet the above specs?

Regards,

Kazu

Hello Kazu,

You can use LTpowerCAD to help you with your design requirement.

These are some of the controllers that were suggested by LTpowerCAD when inputting your specs.

Regards,

Jhun

  • Hi Jhun,

    I get the same products as yours for sure in LTpowerCAD except for LTC4020.

    I exported some recommended circuits showed in Power Stage Design to LTspice and simulated them, but they did not output 600W (24V/25A),

    They could work when the output current reduced to about 300W.

    Is it still difficult to achieve 600W output?

    Regards,

    Kazu

  • FormerMember
    FormerMember on Dec 14, 2022 7:00 PM in reply to Kazu
    +1

    Hi Kazu,

    600W is achievable but you would have bulky components. Plus, you would need >2 MOSFETs in your control and sync MOSFETs since it is a single phase.

    The datasheet has computation guidelines on how to compute for your desired specifications. I would think you'd need a high inductor current >30A saturation. I have ever only seen Wurth inductors having these.

    Regards,

    Jhun