Post Go back to editing

ADP7118 voltage reference tolerance error

Category: Datasheet/Specs
Product Number: ADP7118ACPZN (adjustable)

What is the min/max tolerance error of the ADP7118ACPZN (adjustable) internal voltage reference for the -40°C to 125°C temperature range ?

Can I assume the "output voltage accuracy" specs (±0.8%, -1.2%/+1.5%) for the non-adjustable ADP7118 device would be providing the internal voltage reference errors ?

Thanks.

Edit Notes

Can I assume the "output voltage accuracy" specs (±0.8%, -1.2%/+1.5%) for the non-adjustable ADP7118 device would be providing the internal voltage reference errors ?
[edited by: tmc_EAS at 6:20 PM (GMT -5) on 7 Dec 2022]