Post Go back to editing

LT8390, LT8390A

Thread Summary

The user is designing a Buck-Boost Voltage Regulator using the LT8390 or LT8390A and asks about the use of diodes between BST1/BST2 and INTVCC in the LT8390A. The final answer explains that the diode prevents current from flowing back into the INTVCC, which could damage the bias supply, and allows the high-side voltage to exceed the bias voltage to drive the top FET. The accompanying answers note that the LT8390A has internal diodes, but external diodes are used to ensure fast switching and minimize losses.
AI Generated Content
Category: Datasheet/Specs
Product Number: LT8390

Hello!

I am making a Buck-Boost Voltage Regulator using LT8390 or LT8390A.

Comparing the typical applications listed in the datasheet of the LT8390 and LT8390A, in the case of the LT8390A, BST1 and BST2 are connected to INTVCC through a diode.

I'd like to know why I should use a diode and what the problems would be if I didn't.

Kind regards

Parents
  • FormerMember
    FormerMember
on Nov 28, 2022 1:02 AM
0

Hello,

The diode is used to block current coming back into the INTVCC. You should use diodes that are fast, typically schottky diodes are used as they have very good reverse recovery time, this should minimize the losses.

Regards,

Jhun

  • Hello,

    Thank you for your reply.

    Please can you tell me what happens if I don't add a diode?

    Regards,

  • FormerMember
    FormerMember on Nov 28, 2022 2:18 AM in reply to kurt555
    0

    The current that returns to the Bias Supply might damage the bias, destroying your system.

    Read about how bootstrap circuit works. The diode also lets the Voltage on the High Side to be greater than the Bias in order to drive the top FET.

  • Reply
    • FormerMember
      FormerMember
    on Nov 28, 2022 2:18 AM in reply to kurt555
    0

    The current that returns to the Bias Supply might damage the bias, destroying your system.

    Read about how bootstrap circuit works. The diode also lets the Voltage on the High Side to be greater than the Bias in order to drive the top FET.

    Children