When the datasheet specifies an inductor current ripple in a boost converter, is that value peak-to-peak, or half the peak-to-peak value? I've seen it both ways in textbooks, and the datasheet doesn't specify.
LT8570
Recommended for New Designs
The LT8570 and LT8570-1 are PWM DC/DC converters. The LT8570 contains a 0.5A, 65V power switch, while the LT8570-1 contains a 0.25A, 65V power switch....
Datasheet
LT8570 on Analog.com
When the datasheet specifies an inductor current ripple in a boost converter, is that value peak-to-peak, or half the peak-to-peak value? I've seen it both ways in textbooks, and the datasheet doesn't specify.