I would like to know the main differences between LT3750 and LT3750A.
Can we use one as part "A" and the other one as part "B"?
I would like to know the main differences between LT3750 and LT3750A.
Can we use one as part "A" and the other one as part "B"?
Hello,
I believe there is not much difference with regards to specifications as they still share the same LTSpice model.
Regards,
Nino
Thanks for your reply, I think that also, but the datasheet states this:
"The LT3750A has additional circuitry to guarantee the GATE pin drives low within 200ns of the CHARGE pin being driven below 50mV, the dynamic threshold"
So, I want to know if I can use both of them in the same circuit, due to lead times. I will ask for samples and perform some testing just to be sure.
Hello,
in general all LT parts which have a letter behind their number code (like A, B or C) are pincompatible and offer improvements and/or more robust operation compared to the 'older' part without this letter.
Thanks for your advice, I will use the part with the "A" as preferred and let the other one just in an extreme case.