Category: Hardware
Product Number: Ltc4162-LAD
Hello,
I plan to use the ltc4162-LAD to charge a battery at 4,1V.
does the registers are read at the user programmed values when VIN > 4,5V ? Does the MCU need to program the register at each boot.
Also i need to limit the charging current to 100mA max so i have to use a 0,6 ohms for the RSNSB resistor. Is it ok ?
Thanks for responses