Dear Supporters,
I'm working with the LTC4446, the input signals are generated from uP and the outputs drive four mosfets in full bridge configuration.
The switching frequency is fixed at 1MHz and the selected mosfet are the IRFP140N.
During the EMC test we had a problem with the radiated emission and the problem I found is the ripple on the gate charge and discharge.
The first picture show the scheme and the second picture is the signal on the BG pin of U4.
How I can reduce this ripple?
I tried also with 330nF bootstrap capacitor but the noise is the same.