Post Go back to editing

LTC4060 CHRG status

Thread Summary

The user inquired about the status of the CHRG pin on the LTC4060 when the die temperature reaches 145°C or higher. The final answer confirms that the CHRG pin is pulled to ground in this shutdown state, and charging stops.
AI Generated Content
Category: Datasheet/Specs
Product Number: LTC4060

Hi

I am DFAE in Japan,

When LTC4060 is shutdwon status due to the die temperature  reaches 145℃ or higher,

Is CHRG pin high impeadance status?

Best regards

N.Kokubo

 

Parents Reply Children