Post Go back to editing

Negative output Voltage

Category: Hardware
Product Number: LTC1624

Hello,

I found a component that may be suitable for my application the LTC1624 (please see the DS in this attached). I don't understand very well how it works this electronic assembly :

Is it possible to delete M2/M3 and R3 to have something simpler. I have only +12V (comes from the battery voltage) and I need -5V with 1A to the ouput. Thank you for your helps.

Regards

Yann DOPDF   

Parents Reply Children
  • FormerMember
    0 FormerMember
on Oct 26, 2022 7:58 PM in reply to 206_RC

You would need to find and import the spice model for the component.

  • After working under LTpowerCAD I lost all the schematics of the simulation. Can I work with LTspice (that I know a little better). ? I think it's the same unless I am mistaken.

    Under Mouser I can see 2 models for this component, I think  I must take the second model  Spice2 Model for 'MBRS340T3' and not PSpice I suppose ? 
     

    Do you have links or information to import components under LTspice for simulation ? Thank you for your feedback

    Regard