Post Go back to editing

LTC4291 Port Power deliver

Product Number: LTC4291IUF-1#PBF

Hello,

We Use LTC4291IUF-1#PBF & LTC4292IUj#PBF 4 Port PoE PSE Controller.

We tried to power up an IP camera in Auto mode ,but doesn't work. We did write code to read status registers. We see that PD is detected as status changes when connect & disconnect.

We get port status Rsig too low (PD resistance < 17K).we use only Port 1.Remaining is not use.

When IP Camera Not Connect then Value.

LTC4291 0x00 : 88
LTC4291 0x01 : e4
LTC4291 0x04 : f
LTC4291 0x06 : 0
LTC4291 0x08 : 0
LTC4291 0x0A : 32
LTC4291 0x0C : 6
LTC4291 0x0D : 7
LTC4291 0x0E : 7
LTC4291 0x0F : 7
LTC4291 0x10 : 0
LTC4291 0x11 : 3
LTC4291 0x12 : ff
LTC4291 0x13 : f
LTC4291 0x14 : ff
LTC4291 0x15 : 0
LTC4291 0x16 : 0
LTC4291 0x17 : 80
LTC4291 0x18 : 0
LTC4291 0x1A : 0
LTC4291 0x1B : 64
LTC4291 0x21 : 0
LTC4291 0x2E : 9f
LTC4291 0x2F : 15
LTC4291 0x30 : 0
LTC4291 0x31 : 0
LTC4291 0x32 : 0
LTC4291 0x33 : 0
LTC4291 0x47 : 52
LTC4291 0x48 : 80
LTC4291 0x49 : 0
LTC4291 0x64 : f
LTC4291 0x65 : f
LTC4291 0x6C : 0
LTC4291 0x6F : 7
LTC4291 0x70 : 0
LTC4291 0x74 : 0

When IP Camera Connect then Value.

LTC4291 0x00 : 88
LTC4291 0x01 : e4
LTC4291 0x04 : f
LTC4291 0x06 : 0
LTC4291 0x08 : 0
LTC4291 0x0A : 32
LTC4291 0x0C : 3
LTC4291 0x0D : 7
LTC4291 0x0E : 7
LTC4291 0x0F : 7
LTC4291 0x10 : 0
LTC4291 0x11 : 3
LTC4291 0x12 : ff
LTC4291 0x13 : f
LTC4291 0x14 : ff
LTC4291 0x15 : 0
LTC4291 0x16 : 0
LTC4291 0x17 : 80
LTC4291 0x18 : 0
LTC4291 0x1A : 0
LTC4291 0x1B : 64
LTC4291 0x21 : 0
LTC4291 0x2E : 9c
LTC4291 0x2F : 15
LTC4291 0x30 : 0
LTC4291 0x31 : 0
LTC4291 0x32 : 0
LTC4291 0x33 : 0
LTC4291 0x47 : 52
LTC4291 0x48 : 80
LTC4291 0x49 : 0
LTC4291 0x64 : f
LTC4291 0x65 : f
LTC4291 0x6C : 0
LTC4291 0x6F : 7
LTC4291 0x70 : 0
LTC4291 0x74 : 0

What is Meaning of Rsig too Low and how to solved it ?

Thank you.

Parents Reply
  • The OUT pin is not to have series resistance on this part; as you saw it can affect classification.  There is resistance in your system in parallel with the PD that is causing the signature resistance to appear low.  Please test the PD with the LTC4292/LTC4291-1 demo board and verify this PD is valid.

Children
No Data