Post Go back to editing

LTM4653 doesn't start (again)

Category: Hardware
Product Number: LTM4653
Software Version: -

Hey there, I have an issure with a LTM4653 as 52V to 12V power supply. I got a device back from a customer with the note "will not turn on". After some inspection of the board I recognized that the LTM4653 won't turn on, even if the voltage on the run pin exceeds 1.2V (52V in my case, or 1Meg pull up to Vin, controlled by an open collector for turning it off). So I inverted the level of the switch logic and the LTM4653 starts up correctly after turning on the device but won't turn on again after beeing turned off. I can only get it to work again, if I cut the power. See attached relevant piece of the schematic and screen shot from the osci, showing the behaviour. 12V output turn on with input power but once I cut the voltage to the run pin the device is somehow stuck. Any idea what happened? This is now the 3rd (out of approx 150) boards with this error and I'm somehow lost to what is happening.

Thanks in advance!