Post Go back to editing

LTC3779 modes of operation

Category: Hardware
Product Number: LTC3779

For the LTC3779,

1) Does or can the chip automatically go into continuous mode of operation once the load current demand is high enough? The problem is that in forced continuous mode, no load, the inductor gets very hot.

2) If we then set the chip to be in pulse skip mode, does it stay in pulse skip mode even when a large load current is turned on? 

3) If the chip does not automatically do this, then is there a recommended way to make this switch automatically

    as a function of load current?

4) Also, what is the required common mode range of voltages for the proper use of IAVGSNSP and IAVGNSN differential current sense pins?

Thank you

Top Replies

    •  Analog Employees 
    Oct 19, 2022 +1 verified
    1) Does or can the chip automatically go into continuous mode of operation once the load current demand is high enough? The problem is that in forced continuous mode, no load, the inductor…
Parents
  • 1) Does or can the chip automatically go into continuous mode of operation once the load current demand is high enough? The problem is that in forced continuous mode, no load, the inductor gets very hot.

    During FCM, it is always on continuous mode.

    2) If we then set the chip to be in pulse skip mode, does it stay in pulse skip mode even when a large load current is turned on?

    The switching modes is only during light load operations. It will operate on continuous conduction mode when the load current is high enough.

    3) If the chip does not automatically do this, then is there a recommended way to make this switch automatically

        as a function of load current?

    Read no.2 answer. Thank you.

    4) Also, what is the required common mode range of voltages for the proper use of IAVGSNSP and IAVGNSN differential current sense pins?

    Please read datasheet applications information to help you design your circuit. Refer below snip, it is located on page 21.

Reply
  • 1) Does or can the chip automatically go into continuous mode of operation once the load current demand is high enough? The problem is that in forced continuous mode, no load, the inductor gets very hot.

    During FCM, it is always on continuous mode.

    2) If we then set the chip to be in pulse skip mode, does it stay in pulse skip mode even when a large load current is turned on?

    The switching modes is only during light load operations. It will operate on continuous conduction mode when the load current is high enough.

    3) If the chip does not automatically do this, then is there a recommended way to make this switch automatically

        as a function of load current?

    Read no.2 answer. Thank you.

    4) Also, what is the required common mode range of voltages for the proper use of IAVGSNSP and IAVGNSN differential current sense pins?

    Please read datasheet applications information to help you design your circuit. Refer below snip, it is located on page 21.

Children
No Data