LTM8060
Recommended for New Designs
The LTM8060 is quad 40VIN, 3A step-down Silent Switcher μModule® regulator. The Silent Switcher architecture minimizes EMI while delivering high efficiency...
Datasheet
LTM8060 on Analog.com
Hi,
In LTM8060 product page(AD website) it has been mentioned that LTpower CAD is available for LTM8060.
But in LTpower CAD tool it is not available.
Kindly suggest if I need to update the version?, currently using version 2.7.2.

Hello AD1,
I checked and it is available in the LTpowerCAD library.

Regards,
Nino
Hi Nino,
That's what I am asking it's not showing for me, what should i do?
Thanks,
AD
Hello AD,
I would suggest performing SYNC RELEASE to update your library.
Regards,
Nino
Hi Nino,
I have done SYNC RELEASE two, three times still i can't find LTM8060 in library.
Can you check Input EMI filter design for LTM8060 in your tool?
Operating Condition:
Vin1 , Vin2, Vin3 = 12V
Vout1 = 5V, Iout1 = 2A
Vout2 = 5V, Iout2 = 3A
Vout3 = 5V, Iout3 = 3A
SW Freq = 1.2MHz
EMI specification : CE102 MIL STD
Thanks & regards,
Aravind D