Category: Hardware
Product Number: LTM4680
Software Version: LTpowerplay v1.9.0.0
Hi,
I am using LTM4680 as a single 0.8V 60A output on my board,
The circuit is working and 0.8v can be checked.
Please give me some advice for my below questions.
1. Can I use LTM4680 with the default value in NVM when using it as a single output? (my circuit is designed for two-phase mode)
if not, could you tell me which register I need to change?
2. When I use LTpowerplay to access the LTM4680, it can be detected, but the tool shows two separate outputs,
how can I make the tool recognize the LTM4680-2-Phase circuit?
Best Regards,
Leo