Post Go back to editing

ADP7157 eval board input/output capacitance

Category: Hardware
Product Number: ADP7157CP-04-EVALZ

Hi,

the ADP7157 eval board uses a 10uF input/output cap. However looking up the data on TDK's website (via their DC Bias LTSpice model; I wasn't able to find a chart) it has a capacitance of -60%, or 4uF, at 5V voltage. 5V is well within the operating specs of the ADP7157, but the capacitance is way lower than the minimum capacitance in the datasheet.

The eval board works fine, but I'm confused about the actual minimum capacitance requirement.

Best regards,
David Kraeutmann