LT3042
Recommended for New Designs
The LT3042 is a high performance low dropout linear regulator featuring LTC’s ultralow noise and ultrahigh PSRR architecture for powering noise sensitive...
Datasheet
LT3042 on Analog.com
LTspice
Production
LTspice® is a powerful, fast, and free SPICE simulator software, schematic capture and waveform viewer with enhancements and models for improving the simulation...
LTspice on Analog.com
Does the PG pin of the LT3042 sink current when the device is not powered (IN = EN = PGFB = GND = 0 V)?
The Absolute Maximum Ratings seem to allow this condition (maximum PG pin voltage is 22 V without regard to IN voltage).
The LT3042 model in LTspice suggests PG does not sink current until IN reaches about 1.22 V (maybe the Vgs threshold of the PG output transistor?) I am not sure if this behavior is modeled realistically in LTspice.
Motivation: I want to pull up PG and connect it to an N-MOSFET gate to turn on a relay (driven by a separate power rail). This rail can be high when the LT3042 supply is off. Thus if PG is high-impedance, the relay would wrongly close. (In this case I would need another transistor to break the relay circuit when IN is low.)
Thank you!