Post Go back to editing

LTC4066 number of batteries supported

Category: Hardware
Product Number: LTC4066

Hi,

I have 8 batteries I need to manage for a student CubeSat project and was wondering if I could connect 3 Li-ion batteries to one LTC4066 unit?

The schematic shows 3 battery pins (BAT1, BAT2, BAT3) however none of the application examples indicate the the use of more than one battery/charger unit. I want to make sure it can support 3 batteries/charger unit before I moved forward with the design.

  • Hi EllaH,

    I don't know where you see BAT1, BAT2, BAT3? I found only multiple BAT-pins - and these you have to wire together (I suppose)
    And it is stated that this IC is for one battery.
    You could parallel all 8 batteries, but you can' have them in serial connection.
    For such an application you will also need a balancing IC.
    This circuit is for 5V USB with no boost converter. So it has not enough voltage for serializing batteries.
    Also you can not stack this IC on one another.
    To better assist you, you should describe your input power supply and your wanted output voltage and current.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.