Post Go back to editing

How do I calculate the maximum inductor current when using the LT3473?

Category: Choose a category
Product Number: LT3473

I'm planning to use the LT3473 to boost from 3.5v to 5.5v with 0.65A output current.  How do I calculate the recommended current rating for the inductor?  I'm using the LT3494 for another part of the design and that datasheet describes how to calculate the peak inductor current like this:

Is there an equivalent equation for the LT3473?

Also, regarding the efficiency plot in Figure 3 of the LT3473 datasheet, the efficiency is plotted vs. "Lead Current".  Is Lead Current different than the output current?  If so, how do I calculate that value?

Edit Notes

added details on current and question about "Lead Current"
[edited by: sanjosanjo at 7:59 PM (GMT -4) on 29 Sep 2022]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.