Post Go back to editing

LTC3109

Category: Choose a category
Product Number: LTC3109

Dear all,


I made a pcb design to harvest energy from a voltage drop (>30 mV) that occurs in a trace i have in my PCB.However, when the AC input voltage amplitude reaches 850mV, Vout only outputs a voltage of 5V. When the input voltage is less than 850mV, the output voltage cannot be obtained, and the Vaux output is about 1V.

Thanks.

Edit Notes

Updated post with new ask a question form
[edited by: GenevaCooper at 11:26 AM (GMT -4) on 26 Sep 2022]