Post Go back to editing

Inverting Configuration Using LT8364 - 28Vin and -35Vout

Category: Hardware
Product Number: LT8364

Hello,

I am using the LT8364 to Generate -35V Output from 28V Input. My application load current is low (say, 10mA Max) .  I am using the reference circuit as mentioned in the datasheet. I'm not able to realize the output. 

I was using the LT8361 before and it was a seamless experience generating -35V,I feel LT8364 is a similar device to it.

Please suggest some steps to take for realizing the output.

Reference Circuit being used

Schematic. 

Also would like to understand what the difference between a 100V(LT8361) switch and a 60V(LT8364) will make.

Thank you for the Answer