Post Go back to editing

LTC4040 - Battery discharging limit

Category: Hardware
Product Number: LTC4040

Hello:
We have a board with an LTC4040, a 5V input, a Li-ion battery and a load that is made up of a microprocessor and a communications module.

When we disconnect the input, the battery (through the LTC4040) is responsible for keeping the microprocessor and the communications module powered.

In the absence of input voltage, the battery continues discharging and there comes a time when it is not capable of supplying the load (microprocessor and communications module). The battery voltage is measured, and is maintained at a value of approximately 2.6v.


In this state, although the input voltage of 5v is recovered; however, we found that the battery is no longer recharging, and it stays on indefinitely.
Is this behavior normal? how do we get out of this state?

Thank you and regards,

  • We have also observed that if we disconnect the load, then the battery does start to recharge.

    Do we need to add a switch circuit (MOSFET for instance) al the output, in order to enable the restart of the battery charging process?

    We would appreciate receiving any feedback.

    Thank you.

  • Hello. Other tests ...

    We added a switch circuit (via MOSFET) at the output, but the problem was not completely solved.

    Additionally, we have seen that, when the battery is aprox 2.6v and the 5v input voltage is recovered, a voltage drop is detected on pin PFI, and the battery is not charged.

    We have tested this 2.6v battery in the 2118B demo circuit. A voltage drop is detected again on pin PFI. Same behavior.

    In the 2118B documentation, we saw the possibility to add C6 capacitor in parallel with PFI input (parallel with R27). We addad a C6=100nF and the problem was solved.

    We have not found any advise about max or recommended values for C6. Is there any limitation?

    Thank you and best regards,