Post Go back to editing

Multiple LTM4670/LTM4658

Thread Summary

The user inquired about connecting multiple LTM4670 or LTM4658 modules in parallel to achieve 60A output current. The engineer confirmed that while it is possible to connect them, stability is not guaranteed for configurations exceeding 40A. For 50A output current with low EMI, the LTM4680 or LTM4700 are recommended alternatives, with the LTM4700 providing two 50A channels. The Silent Switcher topology in μModules ensures good EMI performance, and the LTPowerCAD tool can be used to simulate EMI for the application.
AI Generated Content
Category: Hardware
Product Number: LTM4670, LTM4658

Hi,

May I check if I can connect multiple LTM4670s or LTM4658s in parallel to provide more output current (60A)?

Thank you.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.