Hello,
I am using the LT8609 to produce 1.9V from Vin=3.3V.
I want the spread spectrum so I tie the Sync pin to INTVCC.
In the data sheet, it is specified that "Voltage on INTVCC will vary between 2.8V and 3.5V"
In the case of Vin=3.3V, I measure INTVCC=3.05V.
In the data sheet, it is written: "Tie to INTVCC or tie to a voltage between 3.2V and 5.0V for pulse-skipping mode with spread spectrum modulation"
My question is:
Since my INTVCC is 3.05V (lower than the 3.2V to 5.0V specification), can I still tie the SYNC pin to the INTVCC pin and will the spread spectrum correctly work?
Thank you for your help.
Nicolas