Category: Hardware
Product Number: LTC4412
Hi,
I am wondering if 2 x AOD4185 p-channel Mosfet’s are suitable for use in the lowest loss configuration (figure 2 of datasheet).
The required inputs are 12V for the wall adapter and 8V (max) to 5V (min) for the battery cells. Max load current is 2A.
I am also wondering if the AOD4185 is suitable for use as a high-side switch in figure 7 of datasheet, if the supply input is 5v-12V and max load current is 2A.
Thank you