Post Go back to editing

Output voltage LT3798

Category: Choose a category
Product Number: LT3798

Hello, 

I m using the LT3798 on DC/DC configuration. Data are :

Vin = 280V 

Vout = 180V 

Iout_max=800mA

The simulation works well but I have an issue on my board.  The output voltage does not exceed 2V. What can be the root cause of this issue ? 

The Mosfet, transformer, diodes are OK.  The fb resistors are OK too. 

Do you have any idea ? Thank you for the support. 

Here below my schematic :

Parents Reply Children
  • Hello, Thank you for your reply. Unfortunately we don't have much time to perform some tests on the demo board. The output voltage does not reach the desired value and the mosfet continues to break the VDS voltage does not exceed the maximum Mosfet drain voltage. Do you have any suggestions, improvements of my schematic ? Thank you for your support. 

  • Hello, 

    The output voltage issue has been resolved. Now I have another issue which is about the output current control.

    I m using the LT3798 to drive LEDs (80 leds in series) and I want to have an output current regulated of 800mA.

    The problem is that the current is very disturbed and dont reach 800mA. The output current is the blue channel.

    Rsense = 15mohms, Rctrl resistors have been choosen to get more than 800mA.  

    Do you have any idea to resolve this important issue ?

    I am counting on you to give me an answer. Thank you for you support.

    Best regards.