Is there any risk of malfunction if logic system signals (3.3V or 5V) such as EN/UVLO and PWM are input before 24V is supplied to VIN?
As a result of checking the data sheet maximum rating, I think there is no problem, is that correct?
LT3761
Production
The LT3761/LT3761-1 is a DC/DC controller designed to operate as a constant-current source and constant-voltage regulator. It features a programmable internal...
Datasheet
LT3761 on Analog.com
Is there any risk of malfunction if logic system signals (3.3V or 5V) such as EN/UVLO and PWM are input before 24V is supplied to VIN?
As a result of checking the data sheet maximum rating, I think there is no problem, is that correct?
Yes, the logic signals can be present first before Vin. Do not exceed maximum ratings.
Thank you
Thank you